The electrical grid is the backbone of our modern life, delivering power to homes, business and industries. However, with the increasing demand for electricity, renewable energy integration, and the rise of decentralized energy sources, maintaining grid stability has become a complex challenge. This is where Artificial Intelligence (AI) comes into play, offering innovative solutions to optimize grid performance and resilience.
By leveraging optimized AI algorithms and advanced data analytics, grid operators can gain real-time insights into grid operations, monitor critical parameters and automatically detect anomalies for early identification of potential issues enabling prompt intervention to prevent disruption and ensure a stable power supply.
Approach
- This use case is based on the “Electrical Grid Stability” dataset from the UCI Machine Learning Repository.
- The goal was to determine if an electrical grid is stable or not, only using 12 parameters such as production, consumption, time reaction, etc.
- Each sample was measured every 2 seconds, 10 000 real signals were gathered.
- We then used NanoEdge AI Studio to create an N-class classification project based on these inputs to try to predict whether the power grid was stable or unstable.
Sensor
Generic sensors.
Data
2 classes of classification: Stable, Unstable
Signal length: 12 (multi-sensors)
Data rate: 0.5 Hz
Results
N-class classification:
92.35% accuracy, 0.3 Kbytes of RAM, 1.6 Kbytes of Flash memory